This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configure GPIO for use by other Cores on DRA7xx

Intellectual 525 points

Replies: 1

Views: 3335

Hello

I have configured the GPIO6  module which is at base address   0x4805 D000

From the A15 Core. I can access any GPIO  line on Module GPIO6. from Core A15.

When I try to access any of  GPIO line of Module GPIO6 from any other core, the code crashes.

I assumed, we only need to configure and initialize  any GPIO Module once. Then any other Core can access it.?

What I am missing?

Thanks for any Help.

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.