This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Power transmission over 15mm

Prodigy 50 points

Replies: 2

Views: 2291

Hi community,

I'm looking for a solution for Wireless Charging of 5W or 10W, with a distance between coils of about 15mm.

I'm designing both transmitter and Receiver, so no need for standard like WPC, PMA or A4WP, a custom protocol could be used.

15mm gap cannot be reached with Inductive technology like QI or PMA, am I right?

But resonant one, like A4WP, or a custom frequency around few MHz could be used, is that correct?

Is there any TI solution for that system?

Best regards.

Vincent

  • UPDATE -- Oct 31, 2018 WPC Qi range is 5mm max not 15mm.  Below text update.

    Hi Vincent

    We do not have a solution for this distance.  All products are based on the WPC standard and max range is 5mm.

    Best Regards,

    Bill Johns,  Applications Engineer

    Texas Instruments Inc

    Dallas, Texas

    Please click "This resolved my issue" button if this post answers your question.

    For more information on Battery Charger Solutions see Link

    Tip -- Improve search results by including "FAQ" 

  • In reply to Bill Johns:

    Thanks for your quick answer.

    BR
    Vincent

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.