This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51025: BQ51025 EVM DESIGN FILES BGA FOOTPRINT

Prodigy 120 points

Replies: 2

Views: 2041

Part Number: BQ51025

The BQ51025YFP footprint in EVM design files show a 6/10 VIP, hence, a 2mil annular ring on a .062 4-layer stackup . I'm curious, does this not present manufacturing or reliability challenges in a production environment? I'm pretty sure it's the least expensive way to escape the BGA but I'm not sure it even meets IPC Class 1. Is this a recommended layout? 

2 Replies

  • We have not see problems with manufacturing the bq51025 EVM or similar units.

    Best Regards,

    Bill Johns,  Applications Engineer

    Texas Instruments Inc

    Dallas, Texas

    Please click "This resolved my issue" button if this post answers your question.

    For more information on Battery Charger Solutions see Link

    Tip -- Improve search results by including "FAQ" 

  • In reply to Bill Johns:

    I would love to talk to the board house that made the EVM. Mine wants me to got to .4mil laser drill for the VIP  and fan out no more than 1-layer down then adjust dialectric thickness accordingly. Which would be fine except its on one of four rigid segments in a 6-layer rigid-flex design. If I change the dialectric in this one segment it upsets impedance control throughout. I can use different stackups in each rigid segment but that would add even more process steps and cost. I need to keep the production cost down. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.