This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

bqTesla100lp kit, Max distance between the TX and RX possible

Intellectual 745 points

Replies: 1

Views: 2913

Please find the attached file for my implementation.

Regarding the bqTESLA100LP low power wireless power evaluation kit.

With the EVM, the max distance I can achieve, including the plastic, is 8 to 10mm (free space).

For my design requirement, there will be a 20 to 25mm thick rubber in-between the TX and RX. I can't achieve wireless charging at that distance. What is the possible workaround? Could rubber affects the communication signals?

3157.Wireless Charging Concept.ppt

  • The bqTESLA100lp kit and related products are designed to comply with WPC standard see below link.  In this standard the max distance between RX and TX is 5.0mm.

    If you are trying to design a system that is 20 to 25mm it will not comply with WPC.  At this time we are not supporting applications outside the standard.

    ·         Wireless Power Consortium (WPC) Standard and Web site:

    www.wirelesspowerconsortium.com/blog/11/qi-specification-available-for-download

     

    Best Regards,

    Bill Johns,  Applications Engineer

    Texas Instruments Inc

    Dallas, Texas

    For more information on Battery Charger Solutions see Link

    Search "FAQ" on E2E Forum for common questions on battery charger solutions. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.