This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

BQ51050B: Rx tuning and correct Load usage

Prodigy 40 points

Replies: 1

Views: 2112

Part Number: BQ51050B

Hello all,

My questions are about the EVM of BQ51050B - the bq51050BEVM-764

i refer to the below datasheet of this component 

http://www.ti.com/lit/ug/sluua25c/sluua25c.pdf

my questions are :

1) can it use other coil for Rx ?  
2)what capacitors should be replaced for Rx tuning? C1,C2,C3? Is there a formula for that?
3) can I place 4 ohm (25 Watt) resistor as load? Instead of the Emulator depicted in the data sheet in Figure 3?

Thanks 

Igor

  • Hi Igor
    1) can it use other coil for Rx ? --- Bill J-Yes a large number of RX coil are available.
    2)what capacitors should be replaced for Rx tuning? C1,C2,C3? Is there a formula for that?---Bill J - Yes tuning is needed see data sheet for instructions
    3) can I place 4 ohm (25 Watt) resistor as load? Instead of the Emulator depicted in the data sheet in Figure 3?---Bill J - No this would not work. The bq51050B expects to see a voltage and other characters of a battery, if it is only a resistive load it will be declared a shorted battery and unit will shutdown.

    Best Regards,

    Bill Johns,  Applications Engineer

    Texas Instruments Inc

    Dallas, Texas

    For more information on Battery Charger Solutions see Link

    Search "FAQ" on E2E Forum for common questions on battery charger solutions. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.