This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

bq51222: bq51222 evaluation board for 2C lipo

Part Number: bq51222

Hi,

is there an example desing for using the bq51222 to charge a 2C lipo directly at 8.4 V?

And is there an evaluation board available?

And which transceiver chip I should use to connect with bq51222=

Are there aswell example application designs?

Lots of questions, hope for answers.

Cheers,

Constantin

  • Hi Constantin
    is there an example design for using the bq51222 to charge a 2C LiPo directly at 8.4 V?--Bill J - No we do not have a design for this.
    Any Qi Transmitter can be used to power the device.
    For design examples use the bq51221

    Best Regards,

    Bill Johns,  Applications Engineer

    Texas Instruments Inc

    Dallas, Texas

    Please click "This resolved my issue" button if this post answers your question.

    For more information on Battery Charger Solutions see Link

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.