Hello,
I downloaded the IBIS model for buffer sn74cb3q3245 on TI website, but actually I cannot use it properly with the Hyperlynx simulation tool.
Indeed, no matter the pin I choose in the "attribute model" form (see picture), it's always defined as an input.
Did someone experience the same issue ? Any hint how I could fix that ?
Hyperlynx version : LineSim V8.0, build 433
Simulation done using the "free-form schematic" editor.
Hints from the modeling team.
"This is just the standard issue with series pins beingmodeled as series switch, not as buffers (because they don'thave buffers). The user needs to use these pins with theseries switch modeling for the IBIS. They may be able to gettheir simulator to see the series switch info that is alreadyin the IBIS file, by modifying the model_name under the[Pin] section to have '_S' at the end of the model_name."