This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74LV1T34: Output level

Expert 1350 points

Replies: 5

Views: 855

Part Number: SN74LV1T34

Dear E2E member,

1. Does SN74LV1T34 can support TX for UART?

2. I study the datasheet and find the figure 2.

Why the VCC =3.3V but the output level under 3V?

  • Hi Julian,

    The SN74LV1T34 does support Tx for UART.

    I am not sure why the graph on the datasheet looks this way, it does not seem correct. I will make sure to have that updated when possible.

    If you are using the voltage translation between 1.65 to 3.3V, I would recommend using the 2N7001T or maybe the AVC family.

    Thanks!
    - Karan
  • In reply to Karan Kotadia:

    Hi Karan,

    About this question, does TI side have new information?
  • In reply to Julian Chen:

    Hi Julian,

    Is there some other information you were looking for?

    Thanks!
    -Karan
  • In reply to Karan Kotadia:

    Dear Karan,

    If you make sure the fig.2 graph is not correct, I think that is OK to me.

    Because my customer need to confirm it.

    Thanks!

  • In reply to Julian Chen:

    Hi Julian,

    I cannot confirm that those graphs are incorrect because it doesn't mention what load the device is being operated on. The device is also being operated at a really fast speed of 50 MHz so that will also cause it to not reach 3.3 V.

    To fully know how the device will output, you should look at the electrical characteristics section of the datasheet.

    The VOH and VOL levels in these table provide you with the min and max levels of the output based on the current that is being driven. They can also be used to figure out how much drive strength the device has. As for the device working for UART. Yes the device will support UART communication but you cannot expect to operate at very fast speeds with a large load.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.