This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74AUP3G34: SN74AUP3G34DC - Need to know whether the output is push pull

Prodigy 50 points

Replies: 4

Views: 257

Part Number: SN74AUP3G34

SN74AUP3G34DC - Please let me know whether the stated part number is with push pull configuration output? If so i can Pull_Up and Pull-Down output signals ?

  • Hello Ashwin,

    Yes, this is a CMOS device with push-pull outputs that output a high and a low based on the following electrical characteristics listed in the datasheet.

    Thanks!

    - Karan

  • Hello Ashwin, and welcome to the forums!

    To determine if a part is push-pull or open-drain, you can refer to the electrical characteristics table:

    The important things to notice here are:

    (1) The device has both V_OH and V_OL specs - usually indicating a push-pull output architecture. Some open-drain devices do spec V_OH though, so you need to look a little deeper.

    (2) The device is rated to source 4 mA (I_OH = -4 mA) and sink 4 mA (I_OL = 4 mA), which _definitely_ indicates this device has push-pull outputs.


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

  • In reply to Emrys Maier:

    Looks like Karan beat me to it :) Hopefully this helps!


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

  • In reply to Emrys Maier:

    Thank You karan and Emyrs for the detailed description and clarification.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.