This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TXS0108E-Q1: Max leakage current on A / Port?

Intellectual 2200 points

Replies: 2

Views: 126

Part Number: TXS0108E-Q1

Hi team,

Can you provide the data for max leakage current, considering internal pull-up, on A, B port of TXS0108EQPWRQ1?

    -. When 0V (low level) is connected to A port, what is the max leakage current?

    -. When 18V (high level) is connected to A port, what is the max leakage current?

    -. When 0V (low level) is connected to B port, what is the max leakage current?

    -. When 18V (high level) is connected to B port, what is the max leakage current?

Thanks,

Sam Lee

  • Hi Sam,
    We have asked our translation expert to comment. He should be back with you within 24 hours.


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

  • Hi Sam,

    The TXS is a passive device and hence the leakage on the IO ports are not specified.
    If the OE is enabled ( and the Vcca/Vccb powered up), the pullup resistor internally will result in current consumption which will be considered as power supply Icc current.
    With 0V on A or B port , the current consumption will be Vcca/40k and Vccb/40k.

    This is also the reason on the TXS datasheet where the test conditions lists the input and output are left open.

    -Thanks,

    Shreyas

    Watch the Introduction to AXC Family

    Read the app note on Glitch-free Power Sequencing for the AXC family

    Evaluate the AXC8T245 EVM and watch the translation using the EVM

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.