This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

looking for conversion of clipped sine wave to square wave conversion

Intellectual 700 points

Replies: 12

Views: 743

Hi Team

I need one Part number which can convert the clipped sine wave  ( 1MHz and 10 Mhz ) (0.7pk to pk) to Square wave (5V) .

Regards

Nitesh

  • In reply to Jonathan Nguyen:

    Hi Jonny

    Thanks for the reply. It works

    What could be the reason for having Negative pulse is less time period as compared to positive pulse.

    Is it so i need to change the discrete to map it equally.Can you please check and let me know.

    I am attaching the waveform as well as simulation file for the reference.

    Regards

    Nitesh

  • In reply to Nitesh Kumar74:

    Hi Nitesh,

    The reason why the rise/fall times aren't symmetrical is due to the feedback resistor R3 in your circuit.

    Although the datasheet defines the typ Trise/Tfall = 1.5ns (typ), the hysteresis implemented in your circuit will cause some changes in the rise time and fall time as well as propagation delay of the device.

    Regards,
    Jonny

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.