This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TXS02612: VIH at VCCB=1.8V

Expert 5160 points

Replies: 4

Views: 142

Part Number: TXS02612

Hi team,

According to the datasheet, Vih(min) is VCCI-0.2V and it cannot meet Voh(min)=1.4V of SD standard when VCCI is 1.8V (Vih=1.8V-0.2V=1.6V). How can we think about that? Can't this device support the SD standard?

Regards,

Jun

  • Hi Jun,

    It meets the SD standard, but to cover the whole Vcc range from 1.1 to 3.6, it is written that way. I would agree that the writing could have been improved by using a percentage of Vcc to be consistent.
    The internal one shot is tuned to trigger at Vcc/2 and hence 1.4V is enough to trigger the TXS02612 device at 1.8V.
    What is the application( SD standard, data rate etc) as this device doesnt support high speed SD?

    -Thanks,

    Shreyas

    Watch the Introduction to AXC Family

    Read the app note on Glitch-free Power Sequencing for the AXC family

    Evaluate the AXC8T245 EVM and watch the translation using the EVM

  • In reply to ShreyasRao:

    Hello ShreyasRao-san,

    Thank you for your answer.

    BTW, what is the output voltage of A-port at VCCA=3.3V and VCCB=1.8V if the input signal from SD to B-port is 1.4V?

    Regards,

    Jun

  • In reply to Jun Ishida:

    Hi ShreyasRao-san,

    Additionally, can this device support 100MHz clocking speed (SDR50 UHS-I) in spite of the description of max.60MHz in the datasheet?

    Regards,
    Jun
  • In reply to Jun Ishida:

    Hi Jun,

    The output on port A will be at near the Vcca level of 3.3V and is guaranteed to be above the Voh spec when the input on B is at 1.4V.

    AS mentioned in the datasheet, the guaranteed data rate is 60Mhz under the specified loading conditions. 100Mhz is more than 60% above the rated speed. Achieving this data rate is not guaranteed.

    -Thanks,

    Shreyas

    Watch the Introduction to AXC Family

    Read the app note on Glitch-free Power Sequencing for the AXC family

    Evaluate the AXC8T245 EVM and watch the translation using the EVM

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.