• TI Thinks Resolved

TXB0104: Input logic and OE

Prodigy 490 points

Replies: 5

Views: 136

Part Number: TXB0104

Hi Team,

I have two question.

1.Is it okay to input by open drain to TXB0104?

According to datasheet, the device can only translate Push-pull CMOS logic outputs. But I cannot find the mention about input.  

2. Is it necessary to have enable state after VCCA and VCCB are high? or it has no rule about the enable?

TXB0104.pptx

Thanks,

Uchihara