• TI Thinks Resolved

CD40174B: HBM

Intellectual 1275 points

Replies: 3

Views: 72

Hello,

Can you please share HBM data for the following parts?

CD4017BPWR
CD4040BPWR
CD74HC4017QM96EP
CD74HC4059
SN74HC21QPWRG4Q1
SN74LVC1G99-Q1

Thank you

  • Hi,

    I only found the following ESD values on a first round quick search. I will check to see if we have data on the other parts. Some of the CD parts are really old so we might not have the ESD data on them.

    CD4040BPWR : 2kV HBM

    SN74HC21QPWRG4Q1: 2kV HBM

    Thanks!

    -Karan

  • In reply to Karan Kotadia:

    Hi,

    CD4017BE : 2kV HBM

    CD74HC4017QM96: 1kV HBM

    SN74LVC1G99DCU-Q1: 2kV HBM

    I did not have any data on the CD74HC4059 in the system.

    Thanks!

    -Karan

  • In reply to Karan Kotadia:

    Thanks a lot, Karan! 
    One more question though. I've noticed that CD74HC4059 and CD74HC4017QM96 are both "CD74HC40"
    I'm not certain, but if they're using the same ESD protection in the die, then does it follow that both HBM ratings for these devices are 1kV?