• TI Thinks Resolved

LSF0102: Logic forum

Expert 1760 points

Replies: 1

Views: 40

Part Number: LSF0102

Dear Sir/Ms.

When using R2 to design the voltage of Vref_A, is it as follows:

Vref_A=1.5V@VPU=3.3VDevice 1.5-5.5V

Vref_A=1.0V@VPU=3.3V Device 1.0-5.5V

There is also VTH related to the calculation of the value of R2. What is the parameter of VTH?

Best Regards,

Kami Huang