• Resolved

SN5406: SNJ5406FK pins 13 and 19

Intellectual 800 points

Replies: 2

Views: 61

Part Number: SN5406

Hi E2E,

Good day!

The datasheet indicates pins 13 and 19 of the LCCC package as 6A and there is no 4A. May I know which of the two pins should be 4A and which should be 6A?

Looking forward to your response.

Thank you and best regards,

Franz

  • Franz,

    Thanks for pointing this out.

    I will make sure this gets in queue to be updated for next datasheet release.

    Pin 13 should be 4A.

    If this answers your question, please click "This Resolved My Issue"
    Regards,
    Wade

  • In reply to Wade Vonbergen:

    Hi Wade,

    Thank you for your help.

    Best regards,

    Franz