Hi,
I am trying to use three TS5A23160 switches in cascade (SInce it is a dual switch, so 2 such chips in which one switch is left unused).
To my surprise the system doesn't work properly when in slight moist environment (If some voltage falls from 2.5V to 0V at the input of first switch then the same is propagated to the output of third after 3 ms).
3 ms? Wow, it should never be like this. This is too much!!
It works fine when heated a bit. I mean when I heat the switches.
Any idea about what could be happening here?
Thanks,
Ujjwal