This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Equivalent part for the 74LVTH125 with VI DC input voltage as 12V

Other Parts Discussed in Thread: CD4050B, CD4503B, CD4010B

Hi,  

 

We are using 74LVTH125 in one of the our designs. The absolute max DC input voltage VI is 7V. Is there any buffer with DC input voltage as 12V as VI and the supply voltage VCC is 5V.

Please send me the datasheet.  

 

Thanks

Penchalaiah

  • Hello,

    A suitable high voltage buffer would be the CD4010B or the CD4050B. The CD4503B has three state outputs if those are required.

    Please note that we are trying to ensure that all posts are answered. With any new posts, we will be sure answer in a timely manner so that no posts go without a response. We will be closing this thread due to its age. Please feel free to post a new thread if you have additional questions, and we would be very happy to help.

    Best,
    Michael