I will be cascading 10 4094's together to make an 80bit shift register but I need to vary the clocking speed from DC to 1.0 meg. I see that the chip has two outputs QS1 and QS2 to be used depending on "how fast" the clocking speed is. Which output should I use for cascading at this frequency range. I don't want to have to shift between QS1 and QS2 just because I am varying my clock frequency from DC to 1 meg. Thank you!