Hi,
I am using the above device as logic switch as shown in the below schematic. All input, output, enable and Vcc are at 3.3V level. I am seeing below waveform with ch1 at input and ch2 at output of U25. I realize that the IC is more than a digital switch but with level shifting features. The output might not be at Vcc when input is HIGH. however, the drooping (to 2V) seems a bit too much.
can anyone advise on this? thanks.
BR
Gordon