Hi All,
Good morning. I am planning to use SN74LVC541A and I need clarification about the output voltage when there is " NO Input" . This device can accept the input up to 5V with 3.3Vcc. For me the input will be from external/other board ( 5V range) and the output will be connected to the processor which is of 3.3V range. And the /OE pin will be tied to GND to enable always. I want to know whether tri state output will go up to 5V without input( When the other board is not connected)
See the attached4505.sn74lvc541a.pdf datasheet ( Recommended Operating condition --> VO --> Output voltage ).
Waiting for your valuable reply.
Regards,
Saravanan.K