Hello,
i want to use the SN74LVC1G99 as AND logic with 3 State Output.
That means, this truth Table should be valid:
A B C Out
1 1 0 1
So i want to connect A and B with AND logic, and set C as output Enable. Now i do not cleary understand the connection shematic in the datasheet http://www.ti.com/lit/ds/symlink/sn74lvc1g99.pdf on page 5.The first shematic on the top left seems to be the one i need to use, but the two lines in the table down under are not clear to me. Which one is the correct one to use?