Is there possible to find an integrated circuit that can do following: 5V shortly pushed signal on Input0 and permanent switched 5V on Output0 ? If the 5V impulse is pushed on Input1 the Output0 will be released and moved to the Output1. I need 8 Inputs coresponding to 8 Outputs and every one should work separate. As example, with an 8 keys Keyboard. If i touch the no.1 key i need to have 5Volts only on Output0. Touching the key no.2 i need to have 5volts only on Output1 and so on trough Out7. Thank you in advance. With kindly regards.