Hi Team,
Our customer is looking for a 2:1 multiplexer which could use in RMII interface.
I believe there are 4 channels for TX and 4 or 5 channels for RX in RMII, so I think 4 or 8 channel type would be good for their application.
[Q1]
Can the following devices be used in the above RMII signal switching application ?
TS3L110, TS3L301, TS3L500
One thing I was wondering is that these devices does not specify Ron at low input voltage such like under 1.0V. This would mean that low Ron is not guaranteed for these devices.
[Q2]
What would be your recommendation for RMII signal switching application ?
Would SN74CB3Q3257 be a better solution for this app ?
Thanks in advance.
Best Regards,
Kawai