Hi,
I have a question of SN74CBTLV3257.
Our customer are trying to use SN74CBTLV3257 the transmission of USB2.0.
And since it is described as "Bandwidth(MAX)=200MHz" on the product page, can I use?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a question of SN74CBTLV3257.
Our customer are trying to use SN74CBTLV3257 the transmission of USB2.0.
And since it is described as "Bandwidth(MAX)=200MHz" on the product page, can I use?
Best regards,
It can run 200Mhz. What are the voltage levels you will be using?
Thank you for your reply.
Customer is going to be used at 3.3V.
Here is the background of the question.
Maximum data transfer speed of USB2.0 is to 240MHz, TS3USB221A of USB switch will have a bandwidth of 900MHz.
The customer's application is 166MHz transfer. Bandwidth of SN74CBTLV3257 is 200MHz, can not afford.
The customer is concerned about that point.