as pspice model is not available for SN74LVC2G53. i want to use it in my circuit. Biasing the IC under 5V vcc and Gnd. sensor is attached to the COM pin of demux and Y1, Y2 are connected to different ADC. IHN pin is hardwired to GND and A(pin 5) can be high or low. now my question is do i need some thing else to interface or just this setup is enough? signal from sensor can be of 1kHz with 10m to 5 volts.