Hi,
Could you please give us your advice since we have several questions regarding SN74AUC1G125 as follows?
Q1. Power Consumption
Could you please tell us the power consumption in the following conditions?
VCC = 1.8V
Fin = 20MHz
Output Load = 1pF, 2pF, 5pF, 10pF, 15pF
Output Enable = Enable/Disable
Q2. Usage
Could you please tell us what should be noted if we use this part as the clock buffer?
Best Regards,
Kato