In the third paragraph of section 10.2.1.2.1 of the datasheet for LSF0108, (revised October 2014), a reference is made to the signals A3, B4, Ch1/2 and MDIO of Figure 6. Figure 6 contains no such signals however and there are no other figures that appear to be good fits either. The figure in section 10.2.3 seems slightly more relevant, but nothing is labeled Ch1 or "processor".
I think some cleaning up is necessary.
Also, a general comment on the datasheet is the it is quite hard to understand how the device operates based on the datasheet since important internal details are left out and the explanations are confusing. It is much more instructive to read SDLU003 or SCEA035A.
Per