I am designing an SPI Output Expander that will use both TPIC6C595 and 74xx595 shift registers in the same chain (serial output of device one connected to serial input of device two etc.). Knowing that propagation delay and hold time are important for proper operation, I read through several data sheets on various '595 devices. However, in many cases, the minimum propagation delay and hold times are not shown (only typical timing values are given).
Can someone recommend a 74xx595 device that will work properly in the same chain as a TPIC6C595?
Thanks in advance.