Hi!
I am planning to use SN74LVC2T45 to drive a load cap of 200pF at 50MHz. If I short both the channel inputs(3.3V level) and level translate to 5V level outputs(both shorted again), would the device face any problems? Will the device be able to switch quickly enough? Also, could I have any reliability issues for such high load capacitances?
Thanks and Regards,
Subhash