Hello,
I have one of these and I am only using one of the six circuits. The other 5 circuit input pins are shorted to ground.
http://www.digikey.com/product-detail/en/SN74AC14N/296-4301-5-ND/375819
The input is from a voltage divider with a resistor and a light dependent resistor. I measured the output by putting the positive probe of the voltmeter to the output and the negative probe to the negative rail. I get about 125ma. The datasheet shows 24ma per pin.
Since I'm only using one of the 6 circuits does it mean that the output can be 6 x 24ma on one pin? Or am I overdrawing current from it and will damage it long term?
Thanks,
Matt