Hi,
unused control pin of SN74CB3Q3257 and SN74CBTLV16800 has to be connected to GND or VCC.
how about in case of I/O pin? is floating ok?
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
unused control pin of SN74CB3Q3257 and SN74CBTLV16800 has to be connected to GND or VCC.
how about in case of I/O pin? is floating ok?
Thanks in advance.
David,
It would be acceptable to leave the I/O pin floating. Since switches only pass a signal and do not drive an output based on an input threshold like logic gates, there should not be any power wasted by a floating input.
However, I would still recommend connecting the input to ground or VCC so the output is defined in the event that one of the floating channels is selected. This would be especially important if the output of the mux connects to the input of the logic gate.