Hi,
Could I connect the output of CD74ACT541 directly to a TTL input with out any pull up or pull down resistors? If not, what are the recommended values for them?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could I connect the output of CD74ACT541 directly to a TTL input with out any pull up or pull down resistors? If not, what are the recommended values for them?
Thanks.
Mark,
The short answer is 'yes.' The long winded explanation follows.
The CD74ACT541 has a push-pull output architecture, which means it will force a voltage on the output without the need for pull-up or -down resistors. The output high voltage is referred to as V_OH and the low is V_OL. If your system is running at 5 V (TTL), the V_OH for the CD74ACT541 has a minimum of 3.7 V (at some extreme temperatures/currents). The minimum V_OH for the TTL standard is 2 V, so there will be no problem here. The V_OL at 5 V for the CD74ACT541 has a maximum of 0.5 V (also under extreme conditions). The TTL standard only requires 0.8 V max, so there is also no problem with V_OL.
In less extreme circumstances (ie normal use - low current, room temperature), V_OH will be very close to 5 V, and V_OL will be very close to 0 V -- which gives even more headroom for the standard.