Hello,
I'm using the Cd4072B device, TSSOP-14 package. Operating with a 3.3V filtered and no noise supply. The device is bypassed
at pin 14 with a 100n ceramic cap.
Let's look at just device A. Pins 2,3,4,5 are connected to the circuit that senses a high condition (across a 3V LED) when a fault occurs. There is no fault, the LED's are off, the voltage is for all intents and purposes, LOW. Ans so it is at the all the input pins. Some typical noise at 0 to 40mV. Scoping theose inputs shows no noise or oscillation.
Pin 1 is lifted off the pad to ensure nothing could be affecting it. Yet, the output is HIGH. If I fault the detect circuits, that is, actually feed the LED voltage to one of the pins (actually 2.8V) it does not change the output. It's behaving as if there is a high on one of the inputs.
Connecting pin 1 to the pad, and trying to pull it to ground with a 1K resistor brings Vout to 2.9V, but essentially still HIGH. It really is....HIGH.
Can anyone explain this behavior? I've got a whole bunch of boards I need to use this device on, and no one else in the world makes a 4 input OR gate. Is this a single device problem, a batch issue, or...?
Any help, soon, would be very appreciated.
Regards,
Gary