Hello,
What is the worst case supply current for the CD4541 when powered from 12V, 9V, and 6.8V (with auto Reset enabled)? Room temperature is fine...
Thanks,
Eric
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the worst case supply current for the CD4541 when powered from 12V, 9V, and 6.8V (with auto Reset enabled)? Room temperature is fine...
Thanks,
Eric
Thanks for the response. I am actually more concerned about actual operating currents
Example:
Rs = RTC = 10 K Ohm
CTC = 10nF (Fosc approx. 4K)
Auto Reset enabled (LOW)
Master Clear, Mode, Pin A (LOW)
Q and Pin B pulled High
Measured current
Vdd = 12V -> I = 1.6mA
Vdd = 9V -> I = 1.1mA
Vdd = 6.8V -> I = 0.7mA
Are those currents in line with what should be expected???
Thanks,
Eric