I have studied SCBA004C.
I have a 10K pullup on an input to an SN74LVC2244A on a board. VCC is 3.3V.
This input is unused by this board, but the signal is used by other boards in the system. There are pullups also on other boards.
In the system, the driver is an open collector. The combination of multiple pullups are causing the signal to never reach a reliable logic low, and they cannot be changed.
To protect the device when testing the board standalone, I do not want to remove the resistor completely.
I have read that cmos can be pulled up with very large resistor values.
The max input current is +/-5uA, so it should be able to be quite large.
What is the maximum resistor value I can use for this pullup?
Thank You