I've tried a number of searches and can't seem to figure this one out. What's the difference between sn74lvc1g04dryr and sn74lvc1g04dry2?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I've tried a number of searches and can't seem to figure this one out. What's the difference between sn74lvc1g04dryr and sn74lvc1g04dry2?
Hi Mike,
It's a packaging/REEL option, nothing to do with the actual device. Look at page 20 of the datasheet. For DRYR, the device orientation is with pin1 next to the socket holes, the orientation is perpendicular to the tape direction. For DRY2, the device is rotated 90-degrees, the device now parallel to the tape direction.
Pin1 Quadrant
SN74LVC1G04DRY2 SON DRY 6 5000 180.0 8.4 1.65 1.2 0.7 4.0 8.0 Q3
SN74LVC1G04DRYR SON DRY 6 5000 180.0 9.5 1.15 1.6 0.75 4.0 8.0 Q1