This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC244 and SN74AHC244

Other Parts Discussed in Thread: SN74HC244, SN74AHC244

Hello

What is the difference SN74HC244 and SN74AHC244? thanks

Regards,

Nanfang

  • SCAA034: AHC Logic Family says:

    Some advantages of using AHC over HC are:

    • The AHC logic family is almost three times faster than the HC family. The AHC logic family has a typical propagation delay of about 5.2 ns.
    • The AHC logic family allows designers to combine the low-noise characteristics of HCMOS devices with today’s performance levels without the overshoot/undershoot problems typical of higher-drive devices.
    • The AHC family has lower power consumption than the HC family.
    • The output drive is ±8 mA at 5-V VCC and ±4 mA at 3.3-V VCC.