Hi!
I am being asked to lower the supply voltage from 5V to 3.6V on a circuit that has an HCT component in it. In bench testing, the chip appears to work properly, but there is no supporting documentation for HCT at 3.6V. I assume that this is because the HCT inputs are designed to handle TTL and would not be used in a low supply system. The general specifications on the HCT imply that the same die is used for HCT as for CH parts which can be used at 3.6V. Thus, I am not surprised that it works, but I need some sort of confirmation that it will work if the supply = 3.6V and the Vin is 0 - 3.3V, which is almost CMOS input level.
I am hoping for a practical answer rather than an answer limited by the data sheet.
Thanks!