We want to use 74LVC1G123 to derive a High going pulse of width close to ten seconds.
Going by the Calculations in the datasheet , there is no limit provided on the values of REXT and CEXT . Per my requirement i need to use either
1. 1M ohm resistor with a 10uF capacitor OR
2. 10M ohm resistor with a 1uF capacitor
My question is that whether these kind of REXT/CEXT values can be used with 74LVC1G123 and in fact whether it is possible to acheive this value of pulse width using 74LVC1G123
Regards
Jitender