Hi
Should we pull down the input pins that we do not use?
Or can we leave the pin open?
Regards,
Koji Hamamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Should we pull down the input pins that we do not use?
Or can we leave the pin open?
Regards,
Koji Hamamoto
Section 3 of Designing with Logic (SDYA009) says:
In many cases, functions or parts of functions of digital logic devices are unused, for example, when only two inputs of a triple-input AND gate are used. Such parts should not be left unconnected because the undefined voltages at the outside connections result in undefined operational states.
[…]
As a result of the input circuits of bipolar devices, a high level is established at open-circuited inputs. The voltage at such an input corresponds to the threshold voltage of the input circuit (about 1.4 V or 1.1 V with devices from the SN74LS family).
Fairchild's Designing with TTL (AN-363) says:
Inputs are usually tied to VCC through a 1 kΩ to 5 kΩ resistor, since tying them to ground means supplying the IIL current instead of the IIH current. IIL is several orders of magnitude greater than IIH . The resistor is recommended to protect the input against VCC voltage surges and to protect the system against the possibility of the input shorting directly to ground. A single 1k resistor can handle up to 10 inputs.