This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD40107B Open-Drain configuration

Other Parts Discussed in Thread: CD40107B

Hi Team,

I am using the CD40107B NAND Gate in my application in the following manner:

Can you please help answer the following questions:

1. This is not used in the typical open drain configuration, where the output is pulled-up using a resistor and then applied to a load as follows:

Is it ok that the load is part of the pull-up? What are the risks associated with this implementation?

In my implementation, I can use the FET inside the NAND gate to turn on and off my load, but since my load is part of the pull up I am not sure what consequences could result.

2. In the datasheet, there is a graph that I am struggling to understand:

If the output is "low" as it says in the caption, why is the drain-to-source voltage (Vds) at such large voltages?

I am assuming this graph is referring to the following FET:

In my application, Vss is tied to ground, so a Vds of 5V, 10V, or 15V does not seem like a "low" to me..

Thank you for your help here.

Jared