This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT126: SN74AHCT126

Part Number: SN74AHCT126

I designed an interface with 74AHCT126 as shown in the following picture.

The way I designed is to control the enable pins to get either Logic High or  High Z output, so 1A, 2A, 3A are directly connected to 5V. Is there any problem with this design? Should I use a resistor between input A and 5V?

Thank you.