Hello,
I own a old TI PC-100A Thermalprinter (used with TI-59/TI-58/SR-52 Pocket Calculators) from the 1970s which uses three SN96912 to drive the thermal print head. Unfortunatly on circuit seems to be defective - i.e. one row does not work and interchanging two chips moves the column which indicates that its not a print head issue but circuit based issue.
As far as I know is SN96912 a sort of driver circuit
Unfortunatly there are no sources on the web which can provide a datasheet SN96912
Question:
1. Where to obtain datasheet of SN96912 (TI archive ??)
2. Is there a 1:1 replacement (pinout, circuit) for SN96912 ?
Help is really appreciated.
kind regards,
Frank Scherie