Since the "T" in the name refers to ACT devices being compatible with legacy TTL devices, which will not be used in this case, my question is :Will this device function properly using a 4.0V supply? All of the surrounding logic is operating at 3.3V so it will never see a voltage greater than that. I have an existing design that uses the 74ACT139 and would like to reduce the supply voltage but avoid changing the component It seems to operate fine when I've tried it. Is there any change to be expected in the switching time?