Other Parts Discussed in Thread: TXB0102, TXS0101
HI,
We are using TXS0102 to translate our MDC/MDIO lines from 2.5V to 3.3V . What we observed is that the output (3.3V) side signal for MDC is not coming proper.
The pulse rises to 3.3V at the start and then slowly decays to 2V at the end of the pulse. The Pulse level was expected to be staying at 3.3V . instead it is ramping down from 3.3V to 2V which is even less than the input 2.5V pulse,
Please reply what will be the issue .
We tried using TXB0102 but it is not communicating
Regards
Eby Jayan