Hello,
The datasheet for the SN74AHCT1G125 says that the absolute maximum rating for output is VCC+0.5V.
In a footnote, it says "The input and output voltage ratings may be exceeded if the input and output current ratings are observed."
We have a situation (in production) where the device is powered off (VCC = 0V), but the output pin of SN74AHCT1G125 sees a voltage from another device.
This voltage comes from a 5V with a series resistor of 4k7 ohm. It leads to a situation where there is max. 1mA flow into output pin of SN74AHCT1G125, and it sees ~2.0V.
My question: is this situation acceptable because of the low current 1mA going into the output pin of SN74AHCT1G125?
What are the critera I need to look at for this chip and its technology to verify whether damage will occur over some time?