Other Parts Discussed in Thread: CD74HC4049,
Hello,
I need an IBIS model for the CD74HC74M. I could not find one on the website. I need a model that accurately models the output transition times tTLH and tTHL, especially the minimum times. I tried using a model for another part in the same family, the CD74HC4049 since its datasheet showed the same output transition times. But simulations using this model did not appear to be accurate respresentation of the datasheet specs. For example, the datasheet specs tTLH and tTHL for CD74HC4049 (and for CD74HC74) are 15ns max @25C, 19ns max @ -40 to 84C, and 22ns max @ -55 to 125C for 50pF load. But when I simulate the Slow-weak case in Hyperlynx with CD74HC4049 model driving a 50pF capacitor, I only get Trise = 5.844ns and Tfall = 3.920ns which is much less than the datasheet specs. This was for 10 to 90% as specified in the datasheet.
Can you provide an IBIS model that accurately models the minimum tTLH and tTHL output times of the CD74HC74M? As long as it has the same characteristics as the CD74HC74M is all that matters.
Also, please provide what the minimum tTLH and tTHL times of the CD74HC74M should be for a given load so I can confirm by simulation the accuracy of the model that you provide. The datasheet only specifies the maximum tTLH and tTHL times.
Thanks,
Scott