Other Parts Discussed in Thread: SN74LVC3GU04, SN74LVC1G14
Hello.
I recently acquired an SN74HC4060N I intend to use it as a time counter. Following the scheme and formulas of page 6 of the IC's datasheet, I attached a capacitor of C=120nF to pin 9, a resistor or R1=5.6KOhm to pin 10 and another resistor R2=470Ohm to pin11, connecting their three ends. I was expecting a frequency of around 1.2KHz and thus that the Q14/pin 3 would go up after 8 seconds, however surprisingly enough (for me) it did go up but only after 10.5 seconds. I have also tried replacing the capacitor with another one of 100nF, which should have resulted in a higher frequency but still it took 10.5 seconds for pin 3 to go up. I'm using Vcc=5V.
Is this a normal behaviour? Is the IC prepared maybe for a different ratio of R1 and R2, with higher frequencies? Please comment.
Best regards.