Other Parts Discussed in Thread: SN74AXC8T245
Hello, I am planning on using this device for 1.8V to 3.3V translation at 297 Mbps
The first page of the datasheet shows that with this voltage configuration, 320 Mbps is the max data rate.
Further down, the propagation delay for this configuration ranges from 0.5 to 3.9 ns. At 3.9 ns, wouldn't the max data rate be closer to 256Mbps? If the propagation delay happens to fall on the high end, will this data rate be achievable? are there any steps I can take to ensure this device will work at this data rate?
Thanks